This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Compiler Announcement: Release version 21.6.0.LTS available for C2000/CLA



TI is pleased to announce a new C28/CLA compiler version 21.6.0.LTS which includes the following new features.

New features:

- Live Firmware Update feature for C28/CLA firmware update support.

- Generate CRCs over memory ranges.

- Performance improvements:

   - C28 has more efficient data accesses for lower 16-bits of memory when using location attribute or literal addresses.

   - Improved performance for library calls to fmaxf/fminf.

   - Improved performance for MIN/MAX conditionals with volatile variables.

   - The Integer Division Unit (--idiv_support=idiv0) has performance updates for loading integer constants to floating pointer registers.

   - CLA has a performance improvement with more efficiently loading 16-bit constants.

- Enumerated type changes.

- Misra support deprecated.