hello sir,
i have downloaded stepper motor program from ti site .this program will produce 4 signals on IO PORTE0,PORTE1,PORTE2,PORTE3.i have compiled this project and succesfully downloaded this project on to the target but after loading the program when i say run.the DSP is running but iam not getting any signal from the port pins.one more thing is i have downloaded ACI-3 i.e Induction motor control using TMS320LF2407 iam having both asm and C files .The ASM files are working fine but the C files when iam downloading on to the target the same situation it gets downloaded but when i say run the DSP is running but iam not getting the outputs from the pins.pls help me sir.
regards
chakravarthy