Part Number: TMS320F280049C
Other Parts Discussed in Thread: AMC1210, TIDA-01527, TIDM-02009, AMC1311
Dear All,
I am considering the following two methods to implement an isolated resolver interface with TMS320F20049C when applying a resolver for motor control.
Method 1. Apply Resolver-to-digital converter such as AMC1210, AD2S1205 and digital isolator for SPI
Method 2. Apply Discrete Resolver Front-End such as TIDM-02009, TIDA-01527, digital isolator for PWM signal and isloated amplifier such as AMC1311 for sensing.
If there is another way to implement an isolated resolver interface other than the two methods, please advise. And if there are things to consider when applying the above two methods, please advise.
Sincerely,
Eui-heon