This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388S: switch device using syccfg tool

Part Number: TMS320F28388S
Other Parts Discussed in Thread: C2000WARE, , TMS320F28388D, SYSCONFIG

I started an example project "gpio_ex2_toggle" from the "D:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2838x\examples\c28x\gpio\". The original device type is 28388D. I tried to switch the device type to my actual device which is 28388S using syscfg tool.

I clicked the switch button, and selected the CCS Launch Device with TMS320F28388S.

However, after I confirmed the selection, the CCS Launch device was still TMS320F28388D when I opened it again.

Also, the general description of the project was TMS320F28388D as shown below.

It seems that I couldn't change the device type.

Then I created a new project and did the similar operation above. This time, the CCS Launch device was always F28384D.

So, how to switch device type if I want to use syscfg tool?