Other Parts Discussed in Thread: DRV8305-Q1, MOTORWARE
Hi Team,
The customer downloaded the TIDA-01507 reference materials on TI's official website, and directly used the gerber files and schedules inside to make the PCB board, and purchased a PMSM motor with resolver.
The TIDA-01507 reference material also has software information\TIDA-01507\tidcet1\TIDA-01507\sw\solutions\instaspin_servo\boards\TIDA-01507\f28x\f2806xM\projects\ccs\proj_resolver01b. After the board came back, it was tested that the power supply of the board was normal, and the program was compiled and downloaded according to the debugging document of TIDA-01507. He found that the initial program can only compile flash mode programs. According to the instructions "Resolver-based Motor Control Reference Design Supporting BLDC Motors and C2000Tm MCUs", he downloaded it and set the gMotorVars.Flag_Run_Identify variable to 1 in the watch window. The motor does not rotate, the red light D201 of the board is flashing, the yellow light D200 is off or always on, and the green light is off. He did not change anything in this program.
Customer would like to know can the proj_resolver01b project of this design clock directly turn the motor? Still need to change or add something to turn the motor? How to perform motor parameter identification on this board?
The attachment is to download the TIDA-01507 program proj_resolver01b from GTI official website: tidcet1.zip
Thanks,
Annie