Part Number: TMS320F28388D
Hello,
Could XCLKOUT or ECAT_PHY_CLK be used as the clock source for Ethernet PHY? Thank you.
Cindy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Hello,
Could XCLKOUT or ECAT_PHY_CLK be used as the clock source for Ethernet PHY? Thank you.
Cindy
Hi,
At present for TMS320F28388D control card if you see the schematic it uses a fan-out clock buffer to generate the 25MHz phy clocks for Ethernet, Ethercat and device clock input from an oscillator. (pg 3 MCU063B(002)_Sch.PDF)

So if the load on clock does not effect other you can use XCLKOUT or ECAT_PHY_CLK.
Regards,
Yashwant