Part Number: DRV8301-69M-KIT
Hi sir,
I have the DRV8301-69m Kit. and I have three questions on this EVM.
can you help me to clarify them?
1) ADC data is obtained from 0 to 4095, what is the corresponding current value? I'm not sure, but it seems to be between 40A and 60A.
2) In order to put the voltage value of phase ABC into ePWM, the voltage on phase ABC must be divided by the maximum voltage value of the inverter.
After that, the ePWM signal is applied using the division ratio of the CPU clock (the clock of 28069m is 90MHz). What is the maximum voltage value of the inverter?
3) Can I receive the relevant data as a document?
Thanks.
Regards,