This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in loading C28346 via Sci Bootloader - Wrong Echoback

Hi All,

I'm trying to bootload my C28346 with other controller via the sci bootloader, it seems the load ends well. I've programmed a led to blink and it does.

The error is at the echoback I receive from the bootloader. The last byte always returns incorrectly, instead of "00" I receive something different that changes when I change the configuration file. All the other bytes return OK.

I used the hex2000 tool to create the hex file with the "-a", "-boot" and "-sci8" options.

Also, before sending the hex file I synchronize the C28346 to the rate of the master by sending "A" char.

Did anyone else encountered this error? Is it a known bug?

Best regards,

Ron