Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
I have a project that uses functions in the IQmath library. The project runs without issues when I use RAM configurations. I used the "28002x_IQmath_lnk_CProj.cmd" from the C2000Ware directory. I understand that this linker file maps the code for RAM execution. As a next step I replaced the linker file with "28002x_launchxl_demo_flash_lnk.cmd" that also comes from C2000Ware directory. Please note that I am using the LAUNCH-F280025C board as a hardware. The project builds and compile successfully. If I comment the code section that uses IQmath library then the codes executes without any issue. However if I upload the code again with IQmath code included then the CPU goes into some trap. I think that there is some issue in the "28002x_launchxl_demo_flash_lnk.cmd" file relating to IQmath sections that is causing the processor trap. Please guide in fixing this issue. If any one can share flash link command file for F280025C that successfully executes IQmath library functions then it will be very helpful.