Other Parts Discussed in Thread: LAUNCHXL-F28379D, TMDSCNCD28379D
Hi
I want to evaluate the performance of TMS320F28379D, I experimented under the following conditions using Launch-Pad(LAUNCHXL-F28379D).
<condition>
-I evaluated in 16-bit differential input mode using ADCINA0 and ADCINA1.
-To evaluate voltage supply noise influence, ADCINA0 (J3 10pin) and ADCINA1(J7 10pin) connect GND.
<result>
I measured 200 times of ADCRESULT1 the result is following graph.
There was a variation of 21 dec.
Is it necessary to increase the accuracy of VDDA to further improve the accuracy of ADCRESULT?
Or is it necessary to improve Ref voltage accuracy? I think REF5030 in Launch-Pad is sufficient spec, is that correct?

Best regards
Naoki