Part Number: LAUNCHXL-F280025C
Other Parts Discussed in Thread: C2000WARE
Hello,
i couldnot find the bits MCDCR.SYSREF_LOST_MCD_EN=1.
MCDCR consist of :
struct MCDCR_BITS { // bits description
Uint16 MCLKSTS:1; // 0 Missing Clock Status Bit
Uint16 MCLKCLR:1; // 1 Missing Clock Clear Bit
Uint16 MCLKOFF:1; // 2 Missing Clock Detect Off Bit
Uint16 OSCOFF:1; // 3 Oscillator Clock Off Bit
Uint16 rsvd1:1; // 4 Reserved
Uint16 rsvd2:1; // 5 Reserved
Uint16 rsvd3:1; // 6 Reserved
Uint16 rsvd4:1; // 7 Reserved
Uint16 rsvd5:1; // 8 Reserved
Uint16 rsvd6:1; // 9 Reserved
Uint16 rsvd7:6; // 15:10 Reserved
Uint16 rsvd8:16; // 31:16 Reserved
};
AM i missing something here ? could you please help me ?
Thanks
Ushma