Part Number: F28M35H52C
Other Parts Discussed in Thread: UNIFLASH, C2000WARE
Hello:
My client has a problem that during the production of substrate, there was an error in C28 program burning (200 pieces in 2000 pieces)
1、XDS100 has been used for mass production program burning,and burning through uniflash
Error in burning C28


2. Later, My client bought xds200 from Ti mall and used CCS 10.3 to burn C28, but still an error is reported
The error is as follows:
C28xx_0: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00042)
C28xx_0: Error: (Error -1135 @ 0x3FFEAD) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00042)
C28xx_0: Unable to determine target status after 20 attempts
C28xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Can't Run Target CPU:
(Error -1156 @ 0x8050)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.
(Emulation package 9.3.0.00042)
C28xx_0: Breakpoint Manager: Unable to remove requested AET job
C28xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x00004402@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x00004406@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_0: Error occurred during flash operation: Cannot enable while the target is disconnected
C28xx_0: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg
C28xx_0: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
The JTAG circuit is as follows:

3、In E2E forum posts, TI AE suggests that it can be operated into WIR mode. My client don't know how to do that, Can you give operation guide and related source code for us?Thank you