Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE
Hi E2E,
Good day.
Our customer is encountering an error in using the f2838x examples as follows:
I took example 2(position speed calculation) in the eQEP folder in f2838x related examples from c2000ware. Encoder which I use outputs 3600ppr. So, I changed the mech scalar value to 4660. But then the theta mech value for one complete revolution changes from 0 to 31000(final value is not being constant). I found that the final value after completing a revolution is not being constant, It is fluctuating around 31000 + or - 500. And another change in the code which I did is changing the reset mode to max position instead of index position. Could you please give me the source of the error? Also, mention the methods to fix the error? There is no problem with the encoder.
Thank you for your help.
Regards,
Carlo