Part Number: TMS320F28379D
Hi,
Since the beginning I worked on my project, FPU32 and tmu0 are enabled in the project properties (I didn't see before).
I don't want to use fpu32, so I change with "softlib" in the properties ; error, I have this message :
" error #16008-D: file"C:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.4.LTS/lib/rts2800_fpu32.lib<memory.c.obj>" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line"
Can you help ? I don't use file fpu32 function, I just want to import F021_API_F2837xD.lib
Thanks for your help.
Regards,