This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025-Q1: ROM address to store the CLB algorithm

Part Number: TMS320F280025-Q1


Hi

Please help to confirm the ROM address to store CLB algorithm,Thanks!

  • Hi Neal, 

    Can you provide more details on the query? Do you need ROM address range for the device?

    Best Regards

    Siddharth

  • Hi

    Yes, I need to know the address range stored by CLB algorithm. The PN we use is not version C (F280025C), so I think the ROM space of CLB is empty.

    We can read and write our own data, such as standard quantity, fault code into.If I know the range of addresses that the CLB algorithm stores, I can read and write data to that space

    We usually read and write data after initialization, calibration, and failure shutdown. During the normal operation of the system, we do not read and write data.

    So I think it's possible to use Flash to simulate EEPROM for these static working conditions.

    Thanks!

  • Hi

    Yes, I need to know the address range stored by CLB algorithm. The PN we use is not version C (F280025C), so I think the ROM space of CLB is empty.

    We can read and write our own data, such as standard quantity, fault code into.If I know the range of addresses that the CLB algorithm stores, I can read and write data to that space

    We usually read and write data after initialization, calibration, and failure shutdown. During the normal operation of the system, we do not read and write data.

    So I think it's possible to use Flash to simulate EEPROM for these static working conditions.

  • You write the HLC CLB program at every start up!