Part Number: TMS320F28388D
Hello,
We are finishing a design update migrating a F28379D based product to the F28388D for the express purpose of adding an Ethernet interface. I need to verify that our existing1.2V VDD supply has adequate margin. Looking at the data sheet (SPRSP14D) as well as the migration document (SPRACQ1) I do not find adequate information, specifically no details on the CM power consumption.
Generally what I see are statements like "There is not a significant difference in power consumption between the F2838x and F2837x devices, if the same number of peripherals are being utilized", or table entries dictating maximum IDD in operational mode slightly decreasing for the new device?
Can TI provide any further information about additional VDD power consumption when using the CM as a communication processor for transferring data over ethernet?
Thank you.
Mike