This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: LAUNCHXL-F28379D C coding help needed.

Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, C2000WARE

Hi, 

I am using LaunchXL-F28379D using the Simulink support package for quite some time but I've hit few limitations and want to switch to Code Composer Studio i.e. I want to program the board using C coding. 

Now, I've worked with 8051 and AVR microcontrollers using C before but that doesn't seem to be enough to be able to work with F28379D as I am having trouble even with the LED blinking program. I was wondering if there are any resources that can help me in this regard e.g. personal guidance or manuals to program GPIOs or SCI ports or other peripherals. Specifically, I am looking to write an optimization problem into the F28379D Delfino board, that will read input from GPIOs/Serial port/ADCs, perform a constrained optimization problem, and then output some control action from some other GPIOs/Serial port/DAC pins.

Since I am a newbie to this MCU, any help would be appreciated.

Thanks.