This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388S: UL1998/IEC60730 class B or above supported?

Part Number: TMS320F28388S

Dear champs,

I am asking this for our customer.

The user is looking for a low-cost MCU that can support both real-time control and Ethernet for UL1998/IEC60730 class B or higher.

Does TMS320F2838x support IEC60730/UL1998 class B or better?

It seems F2837x can support it up to class C.

So can F2838x support that?

Wayne Huang

  • Hi Wayne,

    Yes, we're targeting the same level of safety with the F2838x as we do on the F2837x. Our safety collateral for F2838x is still a work in progress--we expect to start releasing the documentation and software end of 3Q/early 4Q.

    Whitney