This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: USB Boot and VrefHI for ADC

Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28379D, LAUNCHXL-F28379D

Hello Team,

1. Can I use USB pins (130 and 131) of MCU to the USB connector directly for USB device boot mode without FTDI chip? Please clarify.

In F2839D Eval board, USB to UART  FTDI chip is used. Dedicated USB pins are not used for boot.

Can you share application circuit of USB Boot option?

2. VrefHI andVrefLO pins. 

Aceptable practice is to tie vrefhi to VDDA and Vreflo to VSSA for unused pins.

If I am using all 4 ADC channels (20pins) , how should I connect Vrefhi (A,B,C,D) and Vreflo (A,B,C,D) for external and internal reference modes?

Please clarify,

Kindly Revert.

Thanks,

Vidhya