This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: Problem of using routines

Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: C2000WARE

Dear team:

1、Under the condition of Build3, the positive and negative amplitudes of the output sine alternating current are not equal when my customer uses the routine (TIDM-HV-1PH-DCAC voltage source inverter). But under the condition of Build1, it is possible to output sinusoidal alternating current with equal positive and negative amplitudes. What causes it?

2、Routine: C:\ti\ccs1011\C2000Ware_DigitalPower_SDK_3_02_00_00\solutions\tidm_hv_1ph_dcac\f2837x\ccs\gridconnectedinvlclfltr

Use "gridConnectedInverterLCLFltr_nonpowerSUITE.projectspec", change "SENSING_OPTION" to "1", switch to ADC sampling mode, but still cannot perform AD conversion. What else does he need to change?

Best regards