This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: error #10008-D: cannot find file, even when the linker path is correct

Part Number: TMS320F28335

Hi,

I am trying to build a project in CCSv5 and I am running into an error due to the library file not being found.

<Linking>

"../F28335_NJection.cmd", line 91: error #10008-D: cannot find file "Flash28335_API_V210.lib" in the linking section of the

I also getting warnings for compatibility, however, everything I have read I can ignore these.

Things that I have tried:

I updated my file search path in the C2000 linker to the location of the library, I have also updated the path in the compiler section but that isn't where I am having errors.

I have physically linked in the file by dragging and dropping into the project explorer.

I have physically moved the file into the project folder.

I am not really sure what else to try. Please help.