This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: RTD sensor interface and DACOUT

Part Number: TMS320F28377S

Hi Team,

1. Can RTD sensors be directly interfaced to ADC input pins of MCU TMS320F28377S with signal conditioning (opamp based) referenced to 3V of VrefHi?

2. Dacout A,B and C pins of MCU can be used instead of using a DAC IC?

Kindly clarify.

Thanks and Regards,

Vidhya

  • 3. Humidity sensor same as RTD?

    Kindly revert. 

  • 1. Can RTD sensors be directly interfaced to ADC input pins of MCU TMS320F28377S with signal conditioning (opamp based) referenced to 3V of VrefHi?

    By RTD, I am assuming that you are referring to sensor components like thermistors. If so, then yes the ADC can sense thermistor-controlled voltages that are properly conditioned and buffered into the VREFLO - VREFHI range.

    For ambient sensors that are sampled at a relatively slow rate (like 1 per second or slower), an op-amp would probably be overkill for buffering. You can implement a voltage divider that is buffered using a properly sized capacitor in a charge sharing configuration instead of an op-amp.

    2. Dacout A,B and C pins of MCU can be used instead of using a DAC IC?

    Yes, although care should be taken to not violate the MIN resistive and MAX capacitive load requirements.

    3. Humidity sensor same as RTD?

    Any sensor can be used as long as its output voltage falls within the VREFLO - VREFHI range and is properly buffered.

  • Hello Tlee,

    1. it is not a thermistor. It is resistance temperature detector 3 wire part. How it has to be interfaced to the MCU? Does it need any ADC IC with SPI/I2C communication to the MCU? Or similar to thermistor, it can be directly interfaced to MCU? Please clarify.

    2. OK

    3.OK. Any application note or circuit for interfacing humidity sensors to C2000 MCU? 

    Thanks,

    Vidhya

  • 1. it is not a thermistor. It is resistance temperature detector 3 wire part. How it has to be interfaced to the MCU? Does it need any ADC IC with SPI/I2C communication to the MCU? Or similar to thermistor, it can be directly interfaced to MCU? Please clarify.

    This would ultimately be up to the system engineer (or similar design expert) to determine. From the C2000 MCU perspective, the ADC can sense voltages between VREFLO and VREFHI. If the sensor can be conditioned to output voltages within this supported range and also satisfy the needs of the ADC input model, there would be no disqualifying factor from sampling the sensor circuit using the ADC.

    3.OK. Any application note or circuit for interfacing humidity sensors to C2000 MCU? 

    I am not aware of any such reference material.