Part Number: TMS320F280025C
Hello,
I wrote a Bootloader to update my TMS320F280025C controller. I want to flash16 bytes at the same time.
The flash process begins and the right data were written to the right addresses in the flash. The problem is that the flash process aborts when the address 0x879DB is flashed.
But only the half data are flashed. When I flash an .bin-File that is smaller than it works fine.
Does anybody no where the problem is and how can I fix them?
Here is the Linker-File for my programm:
MEMORY
{
// All length in word (2Byte). All orgin adresses words.
//--- Begin / Boot -------------------------------------------------------------------
BEGIN : origin = 0x00080000, length = 0x00000002
//--- RAM ----------------------------------------------------------------------------
// RAMM0 : origin = 0x00000000, length = 0x00000400
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAM_Command : origin = 0x00000128, length = 0x00000018 // Not deleted on Soft-Reset: Command APP to Bootloader
RAM_APP_TO_BOOT : origin = 0x00000140, length = 0x00000200 // Not deleted on Soft-Reset: APP has write permission: Used for Reset reason, ...
RAM_Boot_To_APP : origin = 0x00000340, length = 0x000000C0 // Not deleted on Soft-Reset: Boot has write permission: Usage ?
// RAMM1 : origin = 0x00000400, length = 0x000003F8
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 // Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory"
RAM_STACK : origin = 0x00000400, length = 0x000003F8
// RAMLS4 : origin = 0x0000A000, length = 0x00000800
// RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAM_DATA : origin = 0x0000A000, length = 0x00001000
// RAMLS6 : origin = 0x0000B000, length = 0x00000800
// RAMLS7 : origin = 0x0000B800, length = 0x00000800
RAM_OSCI : origin = 0x0000B000, length = 0x00001000
// RAMGS0 : origin = 0x0000C000, length = 0x000007F8
RAM_RAM_CODE : origin = 0x0000C000, length = 0x000007F8 // Code that must be executed in RAM ist copied here
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 // Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory"
//--- Reset ----------------------------------------------------------------------------
RESET : origin = 0x003FFFC0, length = 0x00000002
//--- BootROM --------------------------------------------------------------------------
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
//--- FLASH ----------------------------------------------------------------------------
//--- Bootloader -----
// FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE
// FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000
// FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000
FLASH_BOOTLOADER : origin = 0x080002, length = 0x002FFE // Area of the Bootloader
//--- Config Block ----
// FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000
FLASH_CONFIG : origin = 0x083000, length = 0x001000 // Configuration only written in production of the device. By second Binary.
//--- APP -------------
// FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000
// FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000
// FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000
// FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000
// FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000
// FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000
// FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000
// FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000
// FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000
// FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000
FLASH_APP_CRC : origin = 0x084000, length = 0x000100 // Do not use: This block is used for CRC of the Firmware. It is written by an external tool
FLASH_APPLICATION : origin = 0x084102, length = 0x009EFE // Area of the Application (Size = SizeOfFlash - BEGIN - FLASH_APP_CRC)
// FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000
FLASH_RAM_CODE : origin = 0x08E000, length = 0x001000 // Code that will be copied to RAM
//--- Online config ----
// FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 // Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory"
FLASH_ONLINECONFIG : origin = 0x08F000, length = 0x001000 // Reserve: In case we have to write someting on run time. Yes! We also take RSVD. Because it will only be data.
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH_BOOTLOADER, ALIGN(8)
.cinit : > FLASH_BOOTLOADER, ALIGN(8)
.switch : > FLASH_BOOTLOADER, ALIGN(8)
.reset : > RESET, TYPE = DSECT
command : load = RAM_Command, TYPE = NOLOAD // Command APP to Bootloader.
RamAppToBoot : load = RAM_APP_TO_BOOT, TYPE = NOLOAD // RAM APP to BOOT. Will not be deleated on reset.
RamBootToApp : load = RAM_Boot_To_APP, TYPE = NOLOAD // RAM BOOT to APP. Will not be deleated on reset.
.stack : > RAM_STACK
.heap : > RAM_STACK
.init_array : > FLASH_BOOTLOADER, ALIGN(8)
.bss : > RAM_DATA
.bss:output : > RAM_DATA
.bss:cio : > RAM_DATA
.const : > FLASH_BOOTLOADER, ALIGN(8)
.data : > RAM_DATA
.sysmem : > RAM_DATA
osciRAM : > RAM_OSCI
// Allocate IQ math areas:
// IQmath : > RAM_DATA
// IQmathTables : > RAM_DATA
.TI.ramfunc : LOAD = FLASH_BOOTLOADER,
RUN = RAM_RAM_CODE,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
FlashConfig : > FLASH_CONFIG
}
Best regards,
Markus