Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Hi champs,
My customer uses CGT v6.4.6, build project and generate the firmware.out file. He uses hex2000 with below .cmd file and generate one firmware.hex file for SCI firmware upgrade purpose.
Firmware.out
-i
-boot
-o Firmware.hex
-image
-fill 0xffff
-memwidth 8
-romwidth 8
ROMS
{
Flash : origin = 0x100000, length = 0x80000
}
According to my customer, sometimes he modify the software, build project and convert the .out file, and then he fails to complete SCI firmware upgrade process because of unreasonable block size data from PC side, this situation could be solved when he uses newer version of hex2000 to convert same .out file, but not always can be fixed.
Is there any known issues of CGT v6.4.6 causing this kind of problem please? Please advise, thanks for help.
Regards,
Luke