Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: C2000WARE,
Hello everyone,
I have a problem while running my code.
According to my requirement, right after switching on the power I want to blink my red & blue LEDs to blink for 4 second(which is working perfectly) and then right after that I want my buzzer(external device to be beep for 2 seconds) and then off.
So, the problem is with my code is that, whenever the Power is ON the LED and Buzzer are working simultaneously.
I want my buzzer to work after 4 second for 2 second only.
Could you please how can i control the buzzer because I have tried to change the example provided a lot but I was not succeeded with this.
The problem is still the same.
Sharing my code just for reference:
//
// Included Files
//
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//Buzzer code-----------
#include "F2806x_Device.h" // F2806x Headerfile
#include "F2806x_Examples.h" // F2806x Examples Headerfile
#include "F2806x_EPwm_defines.h" // useful defines for initialization
void HRPWM1_Config(Uint16);
void HRPWM1_Config_1(Uint16 period);
Uint16 i,j, DutyFine, n,update;
Uint32 temp;
//Buzzer code-----------
//
// Function Prototypes statements for functions found within this file.
//
__interrupt void cpu_timer0_isr(void);
//logic for LED------------------------------------------------------------------
//variable to count number of timer interrupts
int tim_int_cnts = 0;
//------------------------------------------------------------------
//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
//
InitSysCtrl();
//Buzzer code------------
InitEPwm1Gpio();
//Buzzer code-----------
// Step 2. Initalize GPIO:
// This example function is found in the F2806x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
// InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2806x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
//
InitPieVectTable();
//Buzzer code---------
update = 1;
DutyFine =0;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
// ePWM and HRPWM register initializaition
//
HRPWM1_Config(10); // ePWM1 target, Period = 10
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
//Buzzer code
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &cpu_timer0_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize the Device Peripheral. This function can be
// found in F2806x_CpuTimers.c
//
InitCpuTimers(); // For this example, only initialize the Cpu Timers
//
// Configure CPU-Timer 0 to interrupt every 500 milliseconds:
// 80MHz CPU Freq, 50 millisecond Period (in uSeconds)
//
ConfigCpuTimer(&CpuTimer0, 80, 500000);
//
// To ensure precise timing, use write-only instructions to write to the
// entire register. Therefore, if any of the configuration bits are changed
// in ConfigCpuTimer and InitCpuTimers (in F2806x_CpuTimers.h), the
// below settings must also be updated.
//
//
// Use write-only instruction to set TSS bit = 0
//
CpuTimer0Regs.TCR.all = 0x4001;
//
// Step 5. User specific code, enable interrupts:
//
//
// Configure GPIO34 as a GPIO output pin
//
/* EALLOW;
GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
EDIS;*/
// Logic for LED Blink for 4 second after POWER ON------------------------------------
EALLOW;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
// GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 1;
GpioCtrlRegs.GPBDIR.bit.GPIO39 = 1;
// GpioCtrlRegs.GPBMUX1.bit.GPIO39 = 0;
EDIS;
//------------------------------------------------------------------------------------------------------------
//
// Enable CPU INT1 which is connected to CPU-Timer 0
//
IER |= M_INT1;
//
// Enable TINT0 in the PIE: Group 1 interrupt 7
//
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
//
// Enable global Interrupts and higher priority real-time debug events
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
// HRPWM1_Config_1(0);
// EALLOW;
// SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
// EDIS;
//
// Step 6. IDLE loop. Just sit and loop forever (optional)
//
// for(;;); // was in original code
// logic for LED blinking----------------------------------------------
while(tim_int_cnts < 8)
{
//Wait here until LEd blinks for 4 seconds
// HRPWM1_Config_1(0);
}
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
GpioCtrlRegs.GPBDIR.bit.GPIO39 = 1;
EDIS;
//---------------------------------------------- ----------------------------------------------
DINT;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
HRPWM1_Config(10);
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
//Buzzer Code------------------------------
while ((tim_int_cnts > 7) && (tim_int_cnts < 12))
{
// for(DutyFine =1; DutyFine <256 ;DutyFine ++)
// {
// //
// // Example, write to the HRPWM extension of CMPA
// //
//
// //
// // Left shift by 8 to write into MSB bits
// //
// EPwm1Regs.CMPA.half.CMPAHR = DutyFine << 8;
//
// //
// // Left shift by 8 to write into MSB bits
// //
// EPwm2Regs.CMPA.half.CMPAHR = DutyFine << 8;
//
// //
// // Example, 32-bit write to CMPA:CMPAHR
// //
// EPwm3Regs.CMPA.all = ((Uint32)EPwm3Regs.CMPA.half.CMPA << 16) +
// (DutyFine << 8);
// EPwm4Regs.CMPA.all = ((Uint32)EPwm4Regs.CMPA.half.CMPA << 16) +
// (DutyFine << 8);
//
// //
// // Dummy delay between MEP changes
// //
// for (i=0;i<10000;i++)
// {
//
// }
// }
}
//Buzzer Code------------------------------
HRPWM1_Config_1(0);
}
//
// cpu_timer0_isr -
//
__interrupt void
cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
//
// Toggle GPIO34 once per 500 milliseconds
//logic for LED-----------------------------------------------------------------
if(tim_int_cnts < 8){
GpioCtrlRegs.GPBDIR.bit.GPIO39 ^=0x01;
GpioCtrlRegs.GPBDIR.bit.GPIO34 ^=0x01;
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
GpioDataRegs.GPBTOGGLE.bit.GPIO39 = 1;
tim_int_cnts++;
}
else if((tim_int_cnts > 7) && (tim_int_cnts < 12)){
tim_int_cnts++;
}
else {
//Do nothing
}
//--------------------------------------------------------------------------------------
//
// Acknowledge this interrupt to receive more interrupts from group 1
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
void
HRPWM1_Config(Uint16 period)
{
//
// ePWM1 register configuration with HRPWM
// ePWM1A toggle low/high with MEP control on Rising edge
//
EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
EPwm1Regs.TBPRD = period-1; // PWM frequency = 1 / period
EPwm1Regs.CMPA.half.CMPA = period / 2; // set duty 50% initially
EPwm1Regs.CMPA.half.CMPAHR = (1 << 8); // initialize HRPWM extension
EPwm1Regs.CMPB = period / 2; // set duty 50% initially
EPwm1Regs.TBPHS.all = 0;
EPwm1Regs.TBCTR = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // EPwm1 is the Master
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR; // PWM toggle low/high
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;
EALLOW;
EPwm1Regs.HRCNFG.all = 0x0;
EPwm1Regs.HRCNFG.bit.EDGMODE = HR_REP; // MEP control on Rising edge
EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;
EPwm1Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO;
EDIS;
}
void
HRPWM1_Config_1(Uint16 period)
{
//
// ePWM1 register configuration with HRPWM
// ePWM1A toggle low/high with MEP control on Rising edge
//
EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
EPwm1Regs.TBPRD = period-1; // PWM frequency = 1 / period
EPwm1Regs.CMPA.half.CMPA = period / 2; // set duty 50% initially
EPwm1Regs.CMPA.half.CMPAHR = (1 << 8); // initialize HRPWM extension
EPwm1Regs.CMPB = period / 2; // set duty 50% initially
}
void
InitEPwm(void)
{
// Initialize EPwm1
}
void
InitEPwmGpio(void)
{
#if DSP28_EPWM1
InitEPwm1Gpio();
#endif // endif DSP28_EPWM1
}
#if DSP28_EPWM1
// InitEPwmGpio - This function initializes GPIO pins to function as EPwm pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
void
InitEPwm1Gpio(void)
{
EALLOW;
// Disable internal pull-up for the selected output pins for reduced power
// consumption. Pull-ups can be enabled or disabled by the user.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; // Disable pull-up on GPIO0 (EPWM1A)
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1; // Disable pull-up on GPIO1 (EPWM1B)
// Configure EPWM-1 pins using GPIO regs
// This specifies which of the possible GPIO pins will be EPWM1 functional
// pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // Configure GPIO1 as EPWM1B
EDIS;
}
#endif // endif DSP28_EPWM1
void
InitEPwmSyncGpio(void)
{
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0; // Enable pull-up on GPIO32 (EPWMSYNCI)
// Set qualification for selected pins to asynch only
// This will select synch to SYSCLKOUT for the selected pins.
GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 0;
// Configure EPwmSync pins using GPIO regs
// This specifies which of the possible GPIO pins will be EPwmSync
// functional pins.
GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 2;
// Disable internal pull-up for the selected output pins for reduced power
// consumption
// Pull-ups can be enabled or disabled by the user.
GpioCtrlRegs.GPBPUD.bit.GPIO33 = 1;
GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 2; // Configures GPIO33 for EPWMSYNCO
}
// InitTzGpio - This function initializes GPIO pins to function as
// Trip Zone (TZ) pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
void
InitTzGpio(void)
{
EALLOW;
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (TZ1)
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0; // Enable pull-up on GPIO13 (TZ2)
GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0; // Enable pull-up on GPIO14 (TZ3)
// Set qualification for selected pins to asynch only
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // Asynch input GPIO12 (TZ1)
GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3; // Asynch input GPIO13 (TZ2)
GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3; // Asynch input GPIO14 (TZ3)
// Configure TZ pins using GPIO regs
// This specifies which of the possible GPIO pins will be TZ functional
// pins.
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 1; // Configure GPIO12 as TZ1
GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 1; // Configure GPIO13 as TZ2
GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 1; // Configure GPIO14 as TZ3
EDIS;
}
Regards,
Divya Tripathi