Dear team,
In the TRM, it shows that CAN TX and RX connect internally in Silent mode. Why?
According to Figure 22-2. CAN_MUX, CAN TX and RX should NOT connect internally in Silent mode.
Please help to check it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
In the TRM, it shows that CAN TX and RX connect internally in Silent mode. Why?
According to Figure 22-2. CAN_MUX, CAN TX and RX should NOT connect internally in Silent mode.
Please help to check it.
Susan,
You are correct that there is no reason for the TX & RX to be connected in the Silent mode. What is important to know is that the TX pin is held high all the time while the RX pin is able to receive data. The figures in the TRM are representational only.