Part Number: TMS320F280025-Q1
Other Parts Discussed in Thread: DRV8323, DRV832X, BOOSTXL-DRV8323RS, LAUNCHXL-F280025C
Hi
In debugging 280025 and drv8323 SPI communication, found that has been unable to read the correct register value, please help analyze the reason, thank you!!
Details are as follows:
1. Refer to the routine of 28004x "bootxl-drv8320rs" evaluation board: "lab 07 - speed mode and tuning speed Pi",The driver of drv832x and SPI bus driver communicating with drv832x in this routine are transplanted to my own program,I now use the "launchxl-f280255c" core board with the "bootxl-drv832rs" driver board. The source of the routine is as follows:

However, the nfault pin is not pulled low when measured with a multimeter,To sum up, the reason is that the reading failed,The register values observed during simulation are as follows:

4. After enabling drv832x,When querying the fault of drv832x_ When the bit migration is 1 and reaches 999 times, the program defines an enabletimeout and sets it to 1, which indicates that startup fails.
The waveforms are as follows (blue line: soMi, green line: Simo, yellow line: SCK, magenta: CS)
But I don't know why soMi is always high, which should be the reason for the failure of reading registers. The waveform of Simo may be abnormal.



thanks!