Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Dear expert.
Support last time was very helpful.
However, there are still some problem in the progress, so I am writing to ask additional questions.
I used by 'TMS320F28377D TRAINING KIT'.
I prepared some program to update recent firmware using LFU.
C2000Ware Project 'F2837xD_sci_flash_kernels'
- F2837xD_sci_flash_kernels_cpu01.out : Download firmware on board using Code Composer.
- F2837xD_sci_flash_kernels_cpu01.txt : kernel text file
- blinky_dc_cpu01.txt : application text file
And I connect PC to board with SCI.
PC --------- RS232 Converter(tx, rx) -------------- Training Board(rx, tx)
Step
1. Download .out file to board
2. Setting GPIO 72,84 to boot SCI mode
3. Running prompt
serial_flash_programmer.exe -d F2837xD -k F2837xD_sci_flash_kernels_cpu01.txt -a blinky_dc_cpu01.txt -b 9600 -p COM9
But, It doesn't worked..
Please let me know if there are any additional things to consider in the part I've been working on.
Thanks and regards,
Isaac.