Hi,
Good Day. I have a customer who is working with TMS320F2812EZDSP. Please see below for his query for your reference. Thank you very much.
I am working with the EzDSP evaluation board for the TMS320F2812 and the ADC performance is poor. In my application, I am running the CPU PLL at 45 MHz and scale clock to the ADC at 12.25 MHz. I'm using the PS register at 0. When I perform sequential reads of a DC signal, I am getting noise levels of 4-5 bits out of 12 bit ADC. From the Errata and datasheet is appears the noise level should be limited to 2 bits. I have tried higher PS settings up to 4 with no real improvements. Only when PS goes to 15 do I get to a noise level of 3 bits. Can you assist me on what I am doing wrong or is this within expectation?
Best Regards,
Ray Vincent