Part Number: TMS320F28388D
Hi
I am planning to use the Ethernet peripheral of ARM Cortex core in TMS320F28388D for an application. The data to be processed is around 512kB. The internal RAM which is around 100kB is not sufficient, therefore an external RAM has to be interfaced. But it seems that the External Memory interface(EMIF1/EMIF2) can be accessed only by the C28x cores. Also there is no parallel interface peripheral on ARM core. Please suggest how to interface an external memory from the ARM core.
Best Regards,
Naveen.