Part Number: LAUNCHXL-F28379D
Hello,
I am trying to receive data from an AD2S1205 resolver to digital converter via SPI. I am using the C2000 support package for simulink. There I tried the SPI receive block but failed. If I set up the SPI periphery no clock is put out at the pin. Also the CS pin won´t go low. I tried different SPI examples as well from matlab but they did not work as well on my board. The board is a launchxl-f28379d and I am using the SPI A channel. Do I need to initialize the SPI in the code/ simulink model? Or are there some other tips and tricks to get this running?
Thank you.
In the picture is the timing diagram of the AD2S1205