This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: Detection of EPWM trip sources

Part Number: TMS320F28375D

I've got a project where I would like to use the EPWM trip hardware functionality and have the ability to trip PWM from multiple sources, and then detect the source of the PWM trip after the event occurs.  Currently I'm accomplishing this by manually polling GPIO pin status of the trip sources afterwards in software (see code below), but this has the potential to miss recording the trip source correctly if the trip event is very short duration.  Ideally, I'd like to find a way to query a hardware register that could point me to the source of the trip signal.  Is this possible?

Code of the software polling approach is below:

  // INITIALIZATION (call once)
  //================
  //Select DRV_FAULT & estop as INPUTXBAR1
  XBAR_setInputPin(XBAR_INPUT1, XBAR_INPUT_GPIO_M1);
  XBAR_setInputPin(XBAR_INPUT2, ESTOP_SENSE);

  // Configure TRIP 4 to OR the High and Low trips from both
  // comparator 1, 2 & 3, clear everything first
  EALLOW;
  HWREG(XBAR_EPWM_CFG_REG_BASE + XBAR_O_TRIP4MUX0TO15CFG) = 0;
  HWREG(XBAR_EPWM_CFG_REG_BASE + XBAR_O_TRIP4MUX16TO31CFG) = 0;
  EDIS;

  // Enable Muxes for ored input of CMPSS1H and 1L, mux for Mux0x
  //cmpss1 - tripH or tripL
  XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH_OR_L);

  //cmpss4 - tripH or tripL
  XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX06_CMPSS4_CTRIPH_OR_L);

  //cmpss3 - tripH or tripL
  XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX04_CMPSS3_CTRIPH_OR_L);

  //inputxbar1 trip DRV_FAULT
  XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX01_INPUTXBAR1);

  //inputxbar2 trip estop
  XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX03_INPUTXBAR2);
  //================
 
  // FOREGROUND CHECK (run continuously)
  //================
  // Check for PWM trip
  if((EPWM_getTripZoneFlagStatus(obj->pwmHandle[0]) & EPWM_TZ_FLAG_OST) || (EPWM_getTripZoneFlagStatus(obj->pwmHandle[1]) & EPWM_TZ_FLAG_OST)
      || (EPWM_getTripZoneFlagStatus(obj->pwmHandle[2]) & EPWM_TZ_FLAG_OST)) {

    if(pMotor->faults.indirect.latchFault) {
      pMotor->faults.fault_source.drv = GPIO_readPin(XBAR_INPUT_GPIO_M1);
      pMotor->faults.fault_source.estop = GPIO_readPin(ESTOP_SENSE);
      pMotor->faults.indirect.latchFault = 0;
    }
  }
  //================

  • Hi npaine,

    I see that you use the EPWM_getTripZoneFlagStatus() function to identify if a trip flag has been set. You could also utilize the EPWM_getCycleByCycleTripZoneFlagStatus() function which will tell you what specific CBC trip zone flag occurred [TZCBCFLG register] or the EPWM_getOneShotTripZoneFlagStatus() function which returns the specific one shot trip source/s [TZOSTFLG register]. 

    You can also setup an interrupt every time there is a trip signal (TZEINT register) and then within that determine which specific trip signal occurred and take action accordingly. 

    Best Regards,

    Marlyn