This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: CCS error

Part Number: TMS320F28375D

Hi E2E,

Please help our customer regarding the error encountered in using the TMS320F28375D on CCS, here are the details:

At the moment I am trying to get communication with the TMS320F28375DPZPS. I use Jtag TMS320-XDS100v3_UM-336636 and the program Code Composer to communicate with the Microcontroller. The JTAG and the BOOT Mode are implemented on the board. According to the datasheet, the wait mode must be configured, so that the watchdog reset is not triggered. I get an error message. Despite the correct switch settings, I get the previously mentioned error. I also measured the reset with an oscilloscope, that shows a voltage value of 300mV. Moreover, in Code Composer the Verify function was tested, but there was no error message. Could you possibly help me with this?

Thank you for the assistance.

Regards,
Carlo