Dear Champs,
I am asking this for our customer.
Because standalone XDS110 TMDSEMU110-U is out of stock sometimes and standalone XDS200 is expensive, we suggest using the XDS110 brought out on J102 of F280049/F280025 Launchpad to program legacy F2802x/3x/6x/7x, which has 5-pin JTAG.
Connections as below:
// F280049 Launchpad to user's board
RESET_OUT to nTRST
TMS to TMS
TDI to TDI
TDO to TDO
3.3V to 3.3V
GND to DGND
Remove all shunts/jumpers on J101
CCS uses default XDS110 setting (not 2-pin cJTAG).
Because the user could not succeed in connecting it, we want to confirm if there is anything wrong above.
Wayne Huang