This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: Lowest Power Option

Part Number: TMS320F28384D

Hi C2000 team!

This is a generic C2000 question (not related to the PN). Which ones have the lowest power consumption? Looking at them many of them have the same general specs but I'm sure there are some differences.

- 80pins is preferred

- Ram and Flash don't need to be the highest value so for now up to 512kB is fine

Any recommendations?

Thanks,

Sarah