This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Flags RMLIF0 and AAIF0 in DCAN

Part Number: TMS320F280049


Hello e2e team,

In global interrupt flag registers (CANGIF0) of eCAN there're two bit RMLIF0 and AAIF0, which are set, when a receive-message is lost (RMLIFO) and the send transmission request is aborted (AAIF0). I don't find any flags in  CAN_ES register of DCAN, which are same as these bits.

So I would like to ask whether there are corresponding flags in DCan equal RMLIF0 and AAIF0 in eCAN? Or how I can determine if a received message is lost  and the send transmission request is aborted?

Thank you for your answer.

Best regards,

Thao