Part Number: F28M35H52C
Hi,
Below is my configuration for EPWM9. I have generated SPWM for 3 phase using PWM2 to 7.
I want t generate 50Hz squere wave in sync with SPWM. I use PWM9A to generate 50HZ for Uphase, 9B for W phase.
My configuration is as below.
EALLOW;
// TZ1 Interrupt Enable
EPwm9Regs.TZSEL.bit.OSHT1 = 1; // TZ 1 Source for FORCE PWM HIGH
EPwm9Regs.TZCTL.bit.TZA = TZ_FORCE_HI;
EPwm9Regs.TZCTL.bit.TZB = TZ_FORCE_HI;
EPwm9Regs.TBPRD = 18750; //PWM PERIOD
EPwm9Regs.TBPHS.half.TBPHS = 0; // Phase is 0
EPwm9Regs.TBCTR = 0; // Clear counter
// Setup TBCLK
EPwm9Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm9Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm9Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm9Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm9Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm9Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm9Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm9Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm9Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
// Setup compare
EPwm9Regs.CMPA.half.CMPA = 0; // InitialCompare
EPwm9Regs.CMPB = 0; // InitialCompare
EPwm9Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm9Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm9Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm9Regs.AQCTLB.bit.CBD = AQ_SET;
EPwm9Regs.AQSFRC.bit.ACTSFA = 0x02;
EPwm9Regs.AQSFRC.bit.ACTSFB = 0x02;
EPwm9Regs.AQSFRC.bit.RLDCSF = 0x03;
EPwm9Regs.DBCTL.bit.OUT_MODE = DB_DISABLE; // Dead Band Module is disabled
EDIS;
For generation of Sine wave, I just make PWM pin high whenever there is positive sine ware and Set PWM pin LOW when sine is negative..
Code for 50Hz Squerwageneration;
Actual Requirement is some thing different but this is part of the code where i have to generate 50Hz Squerwave in sync with SPWM.
VUREF_RAM_PWM12 =>> Sine PWM
if(VUREF_RAM_PWM12 >= 0)
{
EPwm9Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm9Regs.AQCTLB.bit.CBU = AQ_SET;
}
else
{
EPwm9Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm9Regs.AQCTLB.bit.CBU = AQ_CLEAR;
}
At PIN 9A : There is 50Hz square wave
At PIN 9B: Only Constant High +3.3V is observed.
I made same configuration to verify in PWM7 module. There also, PWM7A is giving 50Hz sine wave but PWM7B is giving constant high.
can any one help on this?
Re,
Umang