Can I use FlashPro 2000 for compile code to F280004x (generated code by PSIM )
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use FlashPro 2000 for compile code to F280004x (generated code by PSIM )
Jakkapech,
I assume you mean can the FlashPro from Elprotronic be used to load the flash on the F28004x. Yes, the Elprotronic tools support this C2000 MCU for flash programming. The Flash Pro can load .out directly or take in bin files as well.
Best,
Matthew
MatthewPate,
Thank you for your reply, I have further question.
If I use FlashPro for debug software , I have to debug it thorugh CCS or not ?.
Jakkapech,
You will need to use CCS for any debug type operations. The GUI from Elpro will give status of the flash load, and support signals, but it is not a debugger IDE like CCS.
I am not sure that you can use the FlashPro 2000 as the JTAG emulator to connect CCS with the device. Do you have a FlashPro HW currently and can try this out? If not, I believe we have one in our lab, but I'll need a day to find it and try this out.
Best,
Matthew