Part Number: TMS320F28386D
Other Parts Discussed in Thread: C2000WARE
Hello,
In the TRM, it is stated that the digitalization error is 8 clock cycles.
However, in the C2000Ware driverlib code, the function Device_verifyXTAL uses a digitalization error of 6 clock cycles.
Which of the two values is the correct one ?
I think comments in the function should also indicate that the function considers that SYSCLK is currently at 10MHz, otherwise the total error computation is incorrect.
Best regards,
Clément