This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: PWM configuration

Part Number: TMS320F28027

dear

       my customer motor running speed range 1880RPM;  It is planned that the PWM carrier within 1000 RPM is 10K, and that above 1000 RPM is changed to 8K;  

 

At present, the INITIAL configuration of PWM carrier is executed once, and the motor runs normally;  When the motor runs to 1000 RPM or more, the initial configuration function of PWM carrier is called again (to modify the carrier frequency), it cannot be achieved;  

 

What needs to be solved is that when the motor speed reaches 1000 RPM, apart from modifying the carrier frequency by configuring the ePWM cycle register (PWM ->TBPRD = period), are there any other associated register configurations or logic that need to be modified?  Or there are other ways;  

 

The following is the ePWM initial configuration function, refer to InstaSPIN. and advise?thanks in advance

void HAL_setupPwms(HAL_Handle handle,
                   const uint_least16_t systemFreq_MHz,
                   const float_t pwmPeriod_usec,
                   const uint_least16_t numPwmTicksPerIsrTick)
{
  HAL_Obj   *obj = (HAL_Obj *)handle;
  uint16_t   halfPeriod_cycles = (uint16_t)((float_t)systemFreq_MHz*pwmPeriod_usec) >> 1;
  uint_least8_t    cnt;

//  CLK_disableTbClockSync(obj->clkHandle);
  // turns off the outputs of the EPWM peripherals which will put the power switches
  // into a high impedance state.
  PWM_setOneShotTrip(obj->pwmHandle[PWM_Number_1]);
  PWM_setOneShotTrip(obj->pwmHandle[PWM_Number_2]);
  PWM_setOneShotTrip(obj->pwmHandle[PWM_Number_3]);

  for(cnt=0;cnt<3;cnt++)
    {
      // setup the Time-Base Control Register (TBCTL)
      PWM_setCounterMode(obj->pwmHandle[cnt],PWM_CounterMode_UpDown);
      PWM_disableCounterLoad(obj->pwmHandle[cnt]);
      PWM_setPeriodLoad(obj->pwmHandle[cnt],PWM_PeriodLoad_Immediate);
      PWM_setSyncMode(obj->pwmHandle[cnt],PWM_SyncMode_EPWMxSYNC);
      PWM_setHighSpeedClkDiv(obj->pwmHandle[cnt],PWM_HspClkDiv_by_1);
      PWM_setClkDiv(obj->pwmHandle[cnt],PWM_ClkDiv_by_1);
      PWM_setPhaseDir(obj->pwmHandle[cnt],PWM_PhaseDir_CountUp);
      PWM_setRunMode(obj->pwmHandle[cnt],PWM_RunMode_FreeRun);

      // setup the Timer-Based Phase Register (TBPHS)
      PWM_setPhase(obj->pwmHandle[cnt],0);

      // setup the Time-Base Counter Register (TBCTR)
      PWM_setCount(obj->pwmHandle[cnt],0);

      // setup the Time-Base Period Register (TBPRD)
      // set to zero initially
      PWM_setPeriod(obj->pwmHandle[cnt],0);

      // setup the Counter-Compare Control Register (CMPCTL)
      PWM_setLoadMode_CmpA(obj->pwmHandle[cnt],PWM_LoadMode_Zero);
      PWM_setLoadMode_CmpB(obj->pwmHandle[cnt],PWM_LoadMode_Zero);
      PWM_setShadowMode_CmpA(obj->pwmHandle[cnt],PWM_ShadowMode_Shadow);
      PWM_setShadowMode_CmpB(obj->pwmHandle[cnt],PWM_ShadowMode_Immediate);

      // setup the Action-Qualifier Output A Register (AQCTLA) 
      PWM_setActionQual_CntUp_CmpA_PwmA(obj->pwmHandle[cnt],PWM_ActionQual_Set);
      PWM_setActionQual_CntDown_CmpA_PwmA(obj->pwmHandle[cnt],PWM_ActionQual_Clear);

      // setup the Dead-Band Generator Control Register (DBCTL)
      PWM_setDeadBandOutputMode(obj->pwmHandle[cnt],PWM_DeadBandOutputMode_EPWMxA_Rising_EPWMxB_Falling);
      PWM_setDeadBandPolarity(obj->pwmHandle[cnt],PWM_DeadBandPolarity_EPWMxB_Inverted);

      // setup the Dead-Band Rising Edge Delay Register (DBRED)
      PWM_setDeadBandRisingEdgeDelay(obj->pwmHandle[cnt],HAL_PWM_DBRED_CNT);

      // setup the Dead-Band Falling Edge Delay Register (DBFED)
      PWM_setDeadBandFallingEdgeDelay(obj->pwmHandle[cnt],HAL_PWM_DBFED_CNT);
      // setup the PWM-Chopper Control Register (PCCTL)
      PWM_disableChopping(obj->pwmHandle[cnt]);

      // setup the Trip Zone Select Register (TZSEL)
      PWM_disableTripZones(obj->pwmHandle[cnt]);
    }

       // setup the Event Trigger Selection Register (ETSEL)
       PWM_disableInt(obj->pwmHandle[PWM_Number_1]);
       PWM_setSocAPulseSrc(obj->pwmHandle[PWM_Number_1],PWM_SocPulseSrc_CounterEqualZero);
       PWM_enableSocAPulse(obj->pwmHandle[PWM_Number_1]);

  // setup the Event Trigger Prescale Register (ETPS)
  if(numPwmTicksPerIsrTick == 3)
    {
      PWM_setIntPeriod(obj->pwmHandle[PWM_Number_1],PWM_IntPeriod_ThirdEvent);
      PWM_setSocAPeriod(obj->pwmHandle[PWM_Number_1],PWM_SocPeriod_ThirdEvent);
    }
  else if(numPwmTicksPerIsrTick == 2)
    {
      PWM_setIntPeriod(obj->pwmHandle[PWM_Number_1],PWM_IntPeriod_SecondEvent);
      PWM_setSocAPeriod(obj->pwmHandle[PWM_Number_1],PWM_SocPeriod_SecondEvent);
    }
  else
    {
      PWM_setIntPeriod(obj->pwmHandle[PWM_Number_1],PWM_IntPeriod_FirstEvent);
      PWM_setSocAPeriod(obj->pwmHandle[PWM_Number_1],PWM_SocPeriod_FirstEvent);
    }

  // setup the Event Trigger Clear Register (ETCLR)
  PWM_clearIntFlag(obj->pwmHandle[PWM_Number_1]);
  PWM_clearSocAFlag(obj->pwmHandle[PWM_Number_1]);

  // first step to synchronize the pwms
  CLK_disableTbClockSync(obj->clkHandle);//2021.7.8

  // since the PWM is configured as an up/down counter, the period register is set to one-half 
  // of the desired PWM period
  PWM_setPeriod(obj->pwmHandle[PWM_Number_1],halfPeriod_cycles);
  PWM_setPeriod(obj->pwmHandle[PWM_Number_2],halfPeriod_cycles);
  PWM_setPeriod(obj->pwmHandle[PWM_Number_3],halfPeriod_cycles);

  // last step to synchronize the pwms
  CLK_enableTbClockSync(obj->clkHandle);

  return;
}  // end of HAL_setupPwms() function