Other Parts Discussed in Thread: TMS320F2806
Hi all,
We are having some trouble programming our C2000 based custom board with the Spectrum XDS100V2 emulator. We are programming our boards after production, but some micros (TMS320F2806) are dying, approximately 10% of the programmed devices. Each board has 2 micros, and there is no board with both micros death, so if some micro dies, there is always one of the two alive.
We have checked the board before programming and it is OK, but after programming the micro dies, so we think that the problem may be the XDS, maybe some required connection or so.
Any help is welcome. Thanks in advance.