Part Number: TMS320F280025C
I would like information on chaining the output of Tile1 to the input of Tile2. The CLB tool shows connections between the two tiles but is there additional work to be done by the user?
It appears that OUT5 and OUT6 can be directly connected, but what about the other outputs? Do I have to find unused GPIOs to route the signal between GPIO XBARS to connect the
other CLB I/Os ?