This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Tamagawa absolute value encoder check error

Part Number: TMS320F28379D


Dear team:

One of my customer can read the position information of the motor encoder on the IDDKV2.2.1 evaluation board, but he found that check errors often occur. Is there any good way to deal with this?

The position is in the readTformatEncPosition program:

inline void readTformatEncPosition(void)
{

if(tFormat_dataId == PM_TFORMAT_DATAID3)
{
retVal1 = PM_tformat_receiveData(PM_TFORMAT_DATAID3);

crcResult = PM_tformat_getCRC(0, 80, 8,
(uint16_t *)(&tformatData.rxPkts), tformatCRCtable, 10);
crcResult = crcResult ^ (0xFF);

if(!tformat_checkCRC(crcResult, tformatData.crc))
{
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

tFormat_crcError = 1;
runMotor = MOTOR_STOP;


//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

}

//
//Invert the received bit sequence for position and
//turns for actual data
//
position =
((__flip32((uint32_t) tformatData.dataField0) >> 24 ) & 0xFF) |
((__flip32((uint32_t) tformatData.dataField1) >> 16 ) & 0xFF00) |
((__flip32((uint32_t) tformatData.dataField2) >> 8 ) & 0xFF0000);

turns =
((__flip32((uint32_t) tformatData.dataField4) >> 24 ) & 0xFF) |
((__flip32((uint32_t) tformatData.dataField5) >> 16 ) & 0xFF00) |
((__flip32((uint32_t) tformatData.dataField6) >> 8 ) & 0xFF0000);

tFormat_encCmdStatus = ENC_CLOSE;
tFormat_dataId = 0; // reset the ID log

Best regards

  • One of my customer can read the position information of the motor encoder on the IDDKV2.2.1 evaluation board, but he found that check errors

    When I've seen errors it is some sort of noise in the system.  I would suggest double-checking all connectors and make sure any connected probes/scope probes are properly grounded.