Hi expert,
My customer is using F280049 controlCARD for testing and now there are some problems.
Customer's ISR code is contained in RAMLS0LS1LS2LS3LS4LS5. When running the program, it triggers Interrupt_illegalOperationHandler(void). But when customer delete some code in ISR randomly to reduce the size of the ISR, the program no longer triggers Interrupt_illegalOperationHandler(void). The customer has tested it, no matter which part of the code is deleted, the result is the same.
It is a little difficult to understand this phenomenon. So could you please tell me why does this happen? Thanks!
BR
Julia