Part Number: TMS320F280021
Other Parts Discussed in Thread: LAUNCHXL-F280025C
Hello Ti,
quick question bc I'm just choosing an external oscillator for my application featuring the TMS320F280021:
In the Datasheet under point 7.11.3.4.1 ("Crystal Oscillator Parameters") it is stated that CL1, CL2 Load capacitance of the crystal must be between 12pf and 24pF. Here I wonder if or why you specify the CL1 and CL2 (assuming that they refer to the 2 Capacitors in Figure 7-13) instead of the capacitance parameter of the crystal itself. In my understanding, between the 2 capacitors connected to the cystal and the load capcitance of the crystal lies a factor 2 (see e.g. https://www.crystek.com/documents/appnotes/PierceGateLoadCap.pdf). That would mean that if CL1 and CL2 is between 12pF and 24pF, the load capacitance of the Crystal would have to be between 6pF and 12pF.
Below, in Table 7-3, it is furthermore stated that CL1=CL2=12 or 24pF, indicating that you really mean the external capacitors with that range of 12pF-24pF.
Please tell me: does the Parameter of the Crystal have to be between 12pF and 24pF or do the external Capactors connected to it have to be between 12pF and 24pF. From my understanding, there is roughly a factor 2 between those definitions, but feel free to correct me on this.
Cheers,
Dominik