Part Number: LAUNCHXL-F280049C
Hi,
we tried to use the launchpad as a seperate controller board without any connection via USB. So we power the board via the 3V3 connection.
As we need a 5V supply, we set the jumper on JP9 to use the 5V from the Step-Up-regulator U5.(JP1 ..3 are all disconnected)
There we found a very strange behaviour: With the jumper connected, the controller hangs immediately. If the jumper is left open, program works as expected. The 5V are loaded with only a few mA, the 3V3 supply can deliver about 2 A. So I don't think, an overload would be the reason. Any suggestions, what the reason can be?
Regards
Kai