This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Power-cycle required instead of manual reset after flashing

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

When I flash my Launchpad with said chip (Program to flash) the program executes.

After pressing the reset button, the program does not run through. A power cycle resolves the issue and leads to the expected behavior of the reset button.

This issue occurs with the "upp_ex1_sdr_tx"-Example program.

Any hints on why the MCU appears to lock itself out after a reset without a proper power cycle? I haven't had this problem with other programs.

Any help is appreciated as I would like to test the devices without unplugging and plugging them in again for each test.