This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Source, cmd, and header file setting

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Dear TI,

I tried to use the example under the path, C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2837xd\examples\cpu1.

So I put all the cmd, header, and source files in the empty project under the path, C:\ti\c2000\C2000Ware_3_04_00_00\device_support\f2837xd\examples\cpu1,

And when I run the blank main c. file, it has error.

It said it need to include inc/hw_memmap.h.

But after that I add the file, it brings out another error.

 

I think I need to do something wrong.

I attached the project file.

Could please let me know what I did wrong?

NEW_EMPTY_20200803_r01.zip