Part Number: TMDSCNCD28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
Hi Team,
Our customer is currently using the TMDSCNCD28379D controlcard with the docking station and they're currently using the on-chip ADCs. However, they need an extension ADC EVM to use with the controlcard. Besides the analog inputs available in the F28379D, the application requires 4 more differential analog inputs. And they'd also would like to have ~10 analog inputs as a buffer in case they would be needing more in the future.
Can you help us check if there's an extension ADC board already implemented with the control card? Sort of an easy way to solve this query without having to use discrete ADC chips and do all the design and soldering.
Thanks in advance!
Kind Regards,
Jejomar