Hello,
We have to enter the Motor Max Current (A) in the InstaSPIN-FOC GUI for the parameter identification. I am working with TMDSHVMTRINSPIN board using the control card TMDSCNCD28069MISO.
In the PMSM data sheet, there is a rated current (2.7 A) and the maximum current (8.1 A).
Which current should be used for the parameter identification as the maximum current.

Thanks